Full ISOBUS integration
B&R offers an ISOBUS stack for agricultural equipment, providing standardized communication between tractors and implements. ISOBUS is a CAN-based communication protocol that enables machines from different manufacturers to exchange data. As a member of the Agricultural Industry Electronics Foundation (AEF), B&R offers an optimal solution for the industry with the new ISOBUS stack.
- Highlights
- Vendor-independent communication between agricultural machines
- Simulation tools for efficient project development
- Certified hardware
ISOBUS is a CAN-based protocol for data exchange between machines from different manufacturers. As a member of the AEF organization, B&R offers a certified ISOBUS stack solution.
Certified hardware
In addition to the software, the X90 control hardware also complies with the requirements of the ISOBUS standard. B&R has therefore had its system verified by the independent ISOBUS Test Center (ITC). The lab tests confirmed that the X90 controller is suitable for use as an ISOBUS task controller.