![](/fileadmin/ACOPOSmulti65_WEISS-cf5a8528.jpg)
Sistema di azionamento distribuito
Essere in grado di integrare direttamente gli azionamenti nella macchina è un requisito fondamentale per la produzione di macchine modulari. B&R ha progettato il sistema di azionamento distribuito ACOPOSremote per rispondere a questa esigenza, consentendo la realizzazione di soluzioni drive perfettamente ottimizzate sull'applicazione in questione.
Moduli inverter ACOPOSmulti65
Unità di collegamento
Cavi
Accessori
Motornahe Wechselrichter 8CVI
Optimal auf die Anwendung zugeschnittene Antriebslösungen sind eine Grundvoraussetzung für wettbewerbsfähige Maschinen und Anlagen. Dabei stellt die direkte Integration der Wechselrichter in die Umgebung des Aktors - ohne dass dafür zusätzliche Begleitmaßnahmen erforderlich sind - eine ideale Konfiguration dar. Dem trägt B&R mit dem dezentralen Antriebssystem ACOPOSremote Rechnung. Diese Architektur bietet verschiedene Vorteile im Hinblick auf die Projektierung der Maschine.
Weitere Informationen
The ideal topology
One of the most substantial advantages has to do with the hybrid cabling between the inverters themselves. Simply connecting ACOPOSremote drive modules together in a line – the "daisy chain" wiring scheme – results in an uncomplicated and flexible machine architecture where energy is passed from one drive module to the next.
Integrated modularity
All modules in the ACOPOSremote product line are designed with IP65 protection, which makes it possible to mount them directly on the machine. The control cabinet then only has to contain the power supply, high-powered inverter modules and other necessary electrical switching devices. The result is a much easier implementation of modular machine architectures. When optional machine functions are required, they can easily be connected – with the requisite dimensioning of the power supply – to the machine's main line using hybrid cables.
Free motor selection
Because the inverter is separate from the motor, the user is free to select the actuator best suited to his drive solution. This is probably the best type of installation, especially for the linear and torque motors that are becoming more and more prevalent. It prevents the properties of the motor from being negatively influenced, and the maximum possible dynamics remain available throughout.
Homogeneous and compatible
ACOPOSremote drive systems offer the well-known functionality of the ACOPOSmulti drive family and can therefore be integrated homogeneously into a drive solution.
Optimal machine and system configurations are based on the ACOPOSremote – the ideal enhancement for modular drive solutions that require the highest levels of performance and flexibility.
Dezentrale Anschlussbox 8CVE
![](/fileadmin/8CVE28000HC00.00-1.right-ea78fcd7.jpg)
ACOPOSremote 8CVI inverters are usually connected via a hybrid cable by simply arranging the individual modules in a line structure. The demands placed on using a hybrid cable in this way are many. In addition to its main tasks of supplying energy and handling network communication, other aspects such as connector technology, manageability and bending radius also need to be taken into consideration. The sum of these demands results in a reasonable maximum cable diameter, but it ultimately limits the available maximum current for supplying the ACOPOSmulti65 8CVI inverters in this line structure.
In applications where this maximum current is insufficient, the necessary power must be provided in another way, made available to a remote location on-site and then redistributed from there. This is where the 8CVE remote connection box comes in.
Robust and flexible
Like the ACOPOSremote, the 8CVE remote connection box is designed with IP65 protection so it can be mounted directly on the machine. Its robust housing makes it ideal for use in tough environmental conditions and allows the user to flexibly adapt the device's location to the requirements of the respective application.
Separate cable routing means more free space
Because the power supply, the 24 V supply, the safety technology (STO signals) and the POWERLINK network are wired separately, the 8CVE remote connection box can provide a considerable amount of power directly to the machine (up to 30 kW).
Not only that, but it's also possible to use standard cables to implement alternative solutions such as transferring energy using slip rings. This provides the user with the flexibility to work with conventional connector technology while still being able to use remote servo drive technology.
Extensive connection options
The 8CVE remote connection box comes equipped with four hybrid cable outlets, which allows the power to be divided between up to four ACOPOSremote 8CVI inverter line structures.
Classic wiring solutions have also been taken into consideration. The connections necessary for the STO signals (Safe Torque Off) are also included on the 8CVE remote connection box and directly affect the ACOPOSremote 8CVI inverters connected to the hybrid cable outlets.
In addition, the 8CVE remote connection box is equipped with two local I/O connections – another example of exemplary support for modular machine concepts.