The Automation Device Interface allows access to specific functions of B&R devices. The settings of this device can be read out and changed using the B&R Control Center applet in the Control Panel.

  • Features:
  • Changing display-specific parameters
  • Reading out device-specific keys
  • Updating the key configuration
  • Activation of device-specific LEDs on a membrane keypad
  • Reading out or calibrating control devices (e.g. key switch, handwheel, joystick, potentiometer)
  • Reading out temperatures, fan speeds, statistical data and switch positions
  • Reading out operating hours (power-on hours)
  • Reading user settings and factory settings
  • Reading out software versions
  • Updating and backing up BIOS and firmware
  • Creating reports about the current system (support assistance)
  • Setting the SDL equalizer value for the SDL cable adjustment
  • Changing the user serial ID
ADI Control Center screenshots - Examples

B&R Automation Device Interface (ADI) Development Kit

With the ADI Development Kit, functions of the B&R Automation Device Interface (ADI) can be accessed from Windows applications that were created with the following development environments, for example:

  • Microsoft Visual C++ 6.0
  • Microsoft Visual Basic 6.0
  • Microsoft Embedded Visual C++ 4.0
  • Microsoft Visual Studio 2005 (or later)
  • Features:
  • A Microsoft Visual Basic module with declarations for the ADI functions
  • Header files and import libraries for Microsoft Visual C++
  • Help files for Visual Basic and Visual C++
  • Sample projects for Visual Basic and Visual C++
  • ADI DLL (for testing applications if no ADI driver is installed)
ADI Development Kit screenshots (version 3.10)

B&R Automation Device Interface (ADI) .NET SDK

With the ADI .NET SDK, functions of the B&R Automation Device Interface (ADI) can to be accessed from .NET applications created with Microsoft Visual Studio 2005 (or later).

  • Supported programming languages:
  • Visual Basic
  • Visual C++
  • Visual C#
  • Features:
  • ADI .NET class library
  • Help documentation files in HTML Help 1.0 format (.chm file) and MS Help 2.0 format (.HxS file)
  • Sample projects and code snippets for Visual Basic, Visual C++ and Visual C#
  • ADI DLL (for testing applications if no ADI driver is installed)

Vyberte prosím zemi a jazyk

B&R Logo